SBASAZ7 November 2025 AMC0380R
PRODUCTION DATA
The resistive divider at the input of the AMC0380R scales down the voltage applied to the HVIN pin to a ±1V linear full-scale level. This signal is available on the SNSP pin, which is also the input of the analog signal chain.
The high-impedance input buffer on the SNSP pin feeds a second-order, switched-capacitor, feed-forward ΔΣ modulator. The modulator converts the analog signal into a bitstream that is transferred across the isolation barrier, as described in the Isolation Channel Signal Transmission section.