SBAU260 April 2016
Figure 8 provides settings that relate to various delays and timing in sending the commands to the hardware from the software.
Delays are provided to allow a command time to execute before the next command is sent.
NOTE
All timing options are relative to the PC and are not exact timings for execution. These delays are from the time the command is sent by the PC to the next command sent from the PC. The timing of receipt and execution is dependent on USB and receive loop delays.
Figure 8. Command Delay Timing Settings