SBAU432 December   2023 AFE7728D , AFE7768D , AFE7769D

 

  1.   Abstract
  2.   2
  3.   Trademarks
  4. 1Introduction
  5. 2Basic EVM Test Procedures
    1. 2.1 Safety
    2. 2.2 Quality
    3. 2.3 Apparel
    4. 2.4 Hardware and Software Requirements
      1. 2.4.1 Test Equipment Required
      2. 2.4.2 Software Required
  6. 3AFE7769DEVM Setup
    1. 3.1 AFE7769D Hardware Changes
    2. 3.2 AFE7769D Connections
    3. 3.3 AFE7769D Software Setup
    4. 3.4 AFE7769D Programming Method 1: Automated
    5. 3.5 AFE7769D Programming Method 2: Using GUI Mode

AFE7769D Programming Method 1: Automated

  1. Open the AFE77xxD GUI version 0.4. Make sure it looks like Figure 3-3, then click Continue. The “Couldn’t Detect FPGA Reset FTDI. Please reset FPGA manually.” message is expected and can be ignored.
    GUID-20230731-SS0I-QP06-1RZJ-GCGPZPQZRDM7-low.png Figure 3-3 Launching AFE77xxD Latte Software
  2. Wait until the GUI loads. It will look like Figure 3-4.
    GUID-20230731-SS0I-XB3V-PLKG-JRDLWBC5VD9J-low.png Figure 3-4 ReadMe AFE77xxD Latte Software
  3. At the top, click on Latte Mode and navigate to Script Mode, as shown in Figure 3-5.
    GUID-20230731-SS0I-VFLN-NKDW-N1NR0Z9SLPT7-low.png Figure 3-5 Switching to Script Mode
  4. Open the PC802_2T2R_Script.py script on the tree view on the left as shown in Figure 3-6.
    GUID-20230731-SS0I-C5L1-HVTN-MQ5M96ZDQRGX-low.png Figure 3-6 PC802 Script
  5. Run the script by pressing F5 or by clicking Run > Buffer. You should see an output in the log window like that shown in Figure 3-7 signaling the script was run with no errors. After running this script, the LMK_LOCKED LED (D11) turns on if the 122.88 MHz reference from the PC802 is connected after programing the PC802.
    GUID-20230731-SS0I-LZ99-T7PW-8LX3KFS5611L-low.png Figure 3-7 Running the PC802 Script