SBAU434B November 2025 – April 2026
Figure 4-3 shows how the Pages control in the upper-left corner allows access to the other pages in the GUI. Navigate to any of the GUI pages using these controls. Figure 4-3 also shows the ADC Capture page. Use this page to easily configure the most important ADC settings, including the General Configuration and Step Configuration parameters, the sequencer mode, and the number of samples or sequences to capture.
Figure 4-3 ADS125P08 EVM GUI ADC Capture Page - General ConfigurationThe General Configuration tab allows to user to set certain parameters that are used for all steps, including the speed mode, the internal reference voltage, the state of the reference buffer, the state of the input buffer, and the Test DAC range. Additionally, the user can enter the External Reference Voltage if applicable. Finally, the “Ready” box indicates if the GUI is ready to communicate to the ADC (in blue) or if the GUI is busy communicating with the ADC (in orange).
The default option in the sequencer mode dropdown in Figure 4-4 allows the user to capture n conversions of a single step, where n is the number entered in the box in the lower left of the GUI. Alternatively, enable the sequencer to capture n complete sequences of all enabled steps.
Figure 4-4 shows the Step Configuration tab. Use these controls to configure the settings for each individual step. When the sequencer is disabled, only Step 0 is shown.
Figure 4-4 ADS125P08 EVM GUI ADC Capture Page - Step ConfigurationTable 4-1 explains in more detail each field shown in #P_O43_QGR_1HC:
ITEM # | PARAMETER | DESCRIPTION |
|---|---|---|
1 | REF_SEL | Select the reference voltage source to be used with this step |
2 | AINP | Select the measurement channel for the positive input for this step |
3 | AINN | Select the measurement channel for the negative input for this step |
4 | SYS_MON | Select the system monitor option to be measured in this step NOTE: the system monitor takes precedence over the AINP and AINN selections (see #2 and #3 above), and also uses the internal reference regardless of the selection in REF_SEL |
5 | FLTR_OSR | Select the OSR for this step NOTE: the data rate corresponding to this OSR is shown on the right (see #10 below) |
6 | Step Filter Mode | Select the filter mode for this step |
7 | Delay in Tmods | Enter the programmable delay used for this step NOTE: The delay value is measured in modulator clock periods (tMOD), where the modulator clock is selected by the SPEED_MODE field on the General Configuration tab |
8 | TDAC_SEL | Select the location where the Test DAC voltage is output to in this step |
9 | Test DAC (5-bit) | Select the Test DAC voltage to be used for this step NOTE: Enter a value between 0 and 31, which is calculated in volts in the "Test DAC (V)" field on the right (see #13 below) |
10 | Data Rate (SPS) | Data rate relative to the selected OSR (see #5 above) and the SPEED_MODE, assuming the internal oscillator is used NOTE: Select the SPEED_MODE on the General Configuration tab |
11 | Latency (μs) | Calculates the first conversion latency in microseconds NOTE: First conversion latency includes the complete digital filter settling resulting from the FLTR_OSR and Step Filter Mode fields, as well as any additional delay entered in the Delay in Tmods field, if applicable |
12 | Full Scale Voltage | Calculates the full-scale voltage (FSV) for this step |
13 | Test DAC (V) | Calculates the TDAC voltage in volts, where TDAC = TDAC_VAL * TDAC_RANGE NOTE: Set TDAC_VAL on the Step Configuration tab and set TDAC_RANGE on the General Configuration tab |
Enable the ADC sequencer by selecting "Sequencer enabled: continuous mode" from the SEQ_MODE dropdown on the General Configuration tab. Multiple step options appear after selecting this configuration. Additionally, the Capture parameter changes from "Samples" to "Sequences". As a result, the GUI captures and displays the data for the desired number of sequences defined by the user. Figure 4-5 shows how the GUI changes after enabling the sequencer.
Figure 4-5 ADS125P08 EVM GUI ADC Capture Page - Enable SequencerAfter enabling the sequencer, Figure 4-6 shows how clicking on each individual step opens up a new step tab. Clicking on the same step again closes that step tab. This is true for all steps except Step 0, which cannot be disabled.
Figure 4-6 ADS125P08 EVM GUI ADC Capture Page - Enabling Multiple Sequence StepsConfigure each enabled step as shown in Figure 4-7 and described in Table 4-1. Enabling the sequencer also enables the NUM_CONV control on each step page. The NUM_CONV control allows the user to select a specific number of consecutive conversions on that step, instead of taking a single conversion and then immediately switching to the next step. However, the GUI limits the number of sequences to one if the user selects NUM_CONV > 1 on any step page. Figure 4-7 shows this behavior, including a note in the GUI that explains how this limitation is a result of the GUI and not the ADC.
Figure 4-7 ADS125H18 EVM GUI ADC Capture Page - Number of Conversions Field