The following equipment is not included with the EVM kit, but is required for proper
evaluation.
- TSWDC155EVM for capturing the
data from the ADC3910D125EVM
- At least two, low-noise, signal
generators for to provide the ADC sampling clock and an analog input. TI
recommends either of the following signal generators:
- Rohde & Schwarz
SMA100A
- Rohde & Schwarz
SMA100B
- Bandpass filters for the sample
clock and the analog inputs. The filters has a narrow passband within 5%-15% of
the desired bandwidth and minimal insertion loss.
- SMA cables for signal
connections.