SBOS309E August 2004 – December 2024 OPA2830
PRODUCTION DATA
Figure 8-12 shows another approach to mid-supply biasing. This method uses a bypassed divider network in place of the buffer used in Figure 8-10. The impedance is set by the parallel combination of the resistors forming the divider network, but as frequency increases impedance looks more and more like a short due to the capacitor. Generally, the capacitor value must be two to three orders of magnitude greater than the filter capacitors shown for the circuit to properly work.
Figure 8-12 138kHz, 2nd-Order,
High-Pass FilterResults showing the frequency response for the circuit of Figure 8-12 is shown in Figure 8-13.
Figure 8-13 Frequency Response for the Filter of Figure 8-12