SBOS350B December 2006 – December 2024 OPA4830
PRODUCTION DATA
Dual and quad op amps are particularly designed to differential input to differential output applications. Typically, these op amps fall into either ADC input interface or line driver applications. Two basic approaches to differential I/O are noninverting or inverting configurations. Because the output is differential, the signal polarity is somewhat meaningless—the noninverting and inverting terminology applies here to where the input is brought into the OPA4830. Each has advantages and disadvantages. Figure 8-9 shows a basic starting point for noninverting differential I/O applications.
This approach provides for a source termination impedance that is independent of the signal gain. For instance, simple differential filters can be included in the signal path right up to the noninverting inputs without interacting with the amplifier gain. The differential signal gain for the circuit of Figure 8-9 is shown in Equation 6:

Figure 8-9 shows the recommended value of 750Ω. However, the gain can be adjusted using just the RG resistor.
Figure 8-9 Noninverting Differential I/O
AmplifierVarious combinations of single-supply or ac-coupled gains can also be delivered using the basic circuit of Figure 8-9. Common-mode bias voltages on the two noninverting inputs pass on to the output with a gain of 1V/V because an equal dc voltage at each inverting node creates no current through RG, giving that voltage a common-mode gain of 1 to the output.
Figure 8-10 shows a differential I/O stage configured as an inverting amplifier. In this case, the gain resistors (RG) become the input resistance for the source. This configuration provides a better noise performance than the noninverting configuration, but does limit the flexibility in setting the input impedance separately from the gain.
Figure 8-10 Inverting Differential I/O
AmplifierThe two noninverting inputs provide an easy common-mode control input. This control is particularly useful if the source is ac-coupled through either blocking caps or a transformer. In either case, the common-mode input voltages on the two noninverting inputs again have a gain of 1 to the output pins, giving an easy common-mode control for single-supply operation. The input resistors can be adjusted to the desired gain but also change the input impedance as well. The differential gain for this circuit is shown in Equation 7: