SBOU113A June 2011 – January 2023
Figure 4-4 shows the default jumper configuration for the INA226EVM. In general, the jumper settings of the SM-USB-DIG Platform do not need to be changed. You may want to change some of the jumpers on the INA226EVM board to match your specific configuration. For example, you may wish to set a specific I2C address by configuring J3-J6.
Figure 4-4 INA226EVM Default Jumper SettingsTypically, jumper 2 on the INA226EVM is always set to the INT position. When set to the INT position, the SM-USB-DIG Platform provides the supply for the INA226. When this jumper is set to the EXT position, an external supply voltage can be connected to terminal strip T2 to provide the supply for the INA226.
Jumpers 3 through 6 control the I2C address pins for the INA226. These jumpers can set the address for A0 and A1 to either supply, ground, SCL, or SDA. Make sure to only connect one jumper at a time for each address control. Failure to properly connect jumpers can cause shorts or interruptions in the communication lines. For more information on the INA226 addressing, refer to the INA226 product data sheet.
Table 4-1 summarizes the function of the INA226 Test Board jumpers. For most applications, all jumpers should be left in the respective default configurations.
| JUMPER | DEFAULT | PURPOSE |
|---|---|---|
| J2 | INT | This jumper selects whether the VS pin on the INA226 is connected to the VDUT signal generated from the SM-USB-DIG Platform or whether the digital supply pin is connected to terminal T2, allowing for an external supply to power the device. The default INT position connects the VS pin to the VDUT control signal. |
| J3/J4 | GND | This jumper selects the I2C A0 address selection for A0. |
| J5/J6 | GND | This jumper selects the I2C A1 address selection for A1. |