SBVS304B June 2017 – October 2021 TPS7A83A
PRODUCTION DATA
Inrush current is defined as the current into the LDO at the IN pin during start-up. Inrush current then consists primarily of the sum of load current and the current used to charge the output capacitor. This current is difficult to measure because the input capacitor must be removed, which is not recommended. However, Equation 8 can estimate this soft-start current:

where: