SBVS444B January 2025 – June 2025 TPS7B4260-Q1
PRODUCTION DATA
VOUT is set by the voltage at the ADJ/EN pin and the external feedback resistors R1 and R2, according to the following equation.
To ignore the FB pin current error term in the VOUT equation, set the feedback divider current to 100 times the FB pin current (IFB). IFB is listed in the Electrical Characteristics table. This setting provides the maximum feedback divider series resistance, as shown in the following equation.