SCDU028 August   2021

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2General Texas Instruments High Voltage Evaluation Module (TI HV EVM) User Safety Guidelines
  5. 3Information About Cautions and Warnings
  6. 4Features
  7. 5Header Connections and Test Points
  8. 6Setup
  9. 7Layout
  10. 8Schematics
  11. 9Bill of Materials

Header Connections and Test Points

There are 16 headers located around the board with designators J1 through J16. These 3-by-2 headers serve as connections to power planes and to signals of the DUT (U1). Each pin of the DUT has similar header and test point configuration. At four different locations around the board, a legend shows the connections of the pins of the nearby four headers. Figure 5-1 shows a representation of the header associated with pin 1 of U1.

GUID-20210806-CA0I-SRJ2-KK71-ZN5JGJGHW9LB-low.pngFigure 5-1 Header J1 for U1.1

The silkscreen legend represents the connections of the pins of J1. Figure 5-2 shows the pin numbers of this header from this same perspective.

Figure 5-2 Pinout of Headers

Table 5-1 also shows the connections.

Table 5-1 Connections by Header Pin Number
Header pin numberConnection
1No connection
2VDD
3GND
4U1
5GND
6VSS

For all headers J1 through J16, the connections are the same, but are rotated by a multiple of 90° according to their position on the board. A legend is included for each rotation.

There is one 3-by-1 header located near the DUT (J17). Pin 2 of this header is connected to the thermal pad of the DUT. Pin 1 of this header is connected to GND, and pin 3 of this header is connected to VSS.

GUID-20210806-CA0I-KHV7-SHB4-TB5XVTXRBKCZ-low.pngFigure 5-3 Thermal Pad Selector

The connections of J17 are also labeled on the board’s silkscreen layer next to the header.

In addition to headers, multiple test points are located around the board. Black test points (TP18 and TP20-TP26) are connected to GND, the red test point (TP17) is connected to VDD, and the green test point (TP19) is connected to VSS. The remaining blue test points (TP1-TP16 and TP101-TP116) are connected along the signal paths of the pins of U1.

GUID-20210806-CA0I-GPD9-MTBL-T88TKDZ3XR4N-low.pngFigure 5-4 Test Point Colors

The last two digits of the blue test point number represent the pin with which the test point is associated. For example, TP16 and TP116 are both pin 16 of U1.

Table 5-2 shows the test point connections.

Table 5-2 Test Point Connections
DesignatorConnection
TP1

J1.4

TP2

J2.4

TP3

J3.4

TP4

J4.4

TP5

J5.4

TP6

J6.4

TP7

J7.4

TP8

J8.4

TP9

J9.4

TP10

J10.4

TP11

J11.4

TP12

J12.4

TP13

J13.4

TP14

J14.4

TP15

J15.4

TP16

J16.4

TP17

VDD

TP18

GND

TP19

VSS

TP20

GND

TP21

GND

TP22

GND

TP23

GND

TP24

GND

TP25

GND

TP26

GND

TP101

U1.1

TP102

U1.2

TP103

U1.3

TP104

U1.4

TP105

U1.5

TP106

U1.6

TP107

U1.7

TP108

U1.8

TP109

U1.9

TP110

U1.10

TP111

U1.11

TP112

U1.12

TP113

U1.13

TP114

U1.14

TP115

U1.15

TP116

U1.16

Terminal block J35 is the power input for the board. Three power rails (VSS, GND, and VDD) are labeled on the board’s silkscreen layer, indicating the identities of the input pins of the header. Connect the power supply rails at this terminal block to power the board.