Add a decoupling capacitor from VCC to
GND. The capacitor needs to be placed physically close to the device and
electrically close to both the VCC and GND pins. An example layout is
shown in the Layout.
Ensure the capacitive load at the output is ≤
70pF. This is not a hard limit, however it establishes peak performance. This
can be accomplished by providing short, appropriately sized traces from the
SN74HCS7002-Q1 to the receiving
device.
Ensure the resistive load at the output is larger
than (VCC / 25mA) Ω. This ensures that the maximum output current
from the Absolute Maximum Ratings is not violated. Most CMOS inputs
have a resistive load measured in megaohms; much larger than the minimum
calculated above.
Thermal issues are rarely a concern for logic
gates, however the power consumption and thermal increase can be calculated
using the steps provided in the application note, CMOS Power Consumption
and Cpd Calculation