SCLS788B January 2020 – October 2026 SN74HCS7266
PRODUCTION DATA
In this application, a 2-input XNOR gate is used as a phase difference detector as shown in Figure 8-1. The remaining three gates can be used for other applications in the system, or the inputs can be grounded and the channels left unused.
The SN74HCS7266 is used to identify phase difference between a reference clock and another input clock. Whenever the clock states are different, the XNOR output will pulse LOW until the clocks return to the same state. The output is fed into a low-pass filter to obtain a DC representation of the phase difference.
Typically, clock signals have fast transition rates, but additional filtering can be added to the clock signals which can lead to slower transitions rates. This makes the SN74HCS7266 ideal for the application because it has Schmitt-trigger inputs that do not have input transition rate requirements.