SCPS301C September 2024 – April 2026 TPLD801-Q1
PRODUCTION DATA
The TPLD801-Q1 has a power-on reset (POR) macro-cell to ensure correct device initialization and operation of all macro-cells in the device. The purpose of the POR circuit is to have consistent behavior and predictable results when the VCC power is first ramping to the device, and also while the VCC is falling during power-down. To accomplish this goal, the POR drives a defined sequence of internal events that trigger changes to the states of different macro-cells inside the device, and finally to the state of the I/O pins.
The power-on Reset (POR) macro-cell will produce a logic High signal as an output when the device power supply (VCC) rises to approximately VPORR and device completely starts up. All outputs are in high impedance state and chip starts loading data from OTP. The reset signal is released for internal macro-cells and all the registers are initialized to their default states. Figure 7-20 shows POR system generates a sequence of signals that enable certain macro-cells.
As shown in Figure 7-20, after the VCC has start ramping up and crosses the VPORR threshold: