SDAA041 January 2026 TPSM33620-Q1
While the TPSM33620-Q1 achieves EMC against the conducted EMI standards with the use of filtering elements, radiated EMI is often a trickier problem to tackle. Radiated EMI consists of emissions that affect systems not electrically connected to the potential emitter. As such, the CISPR guidelines for radiated EMI can encapsulate frequencies beyond 1GHz and are measured with sensitive antennae away from the device. Devices that meet EMC with conducted standards can still fail the counterpart radiated standards as the techniques used to achieve conducted EMC along electrical lines cannot affect the radiation noise of electromagnetic waves in space. Achieving radiated EMC focuses more on identifying and limiting the effectiveness of the noise sources that radiate EMI.
Like conducted EMI, the sources of radiated EMI lie with the discontinuous currents and voltages in the buck converter’s operation. As previously discussed with differential-mode noise, high di/dt currents propagate through the loop created by CIN, Q1, and Q2 due to the switching nature of the device. Through Ampere’s Law, the time-varying current in the loop generates a magnetic field that is a main contributor to radiated EMI noise. By increasing the loop size, parasitic inductance, or current, the flux and magnetic field through this loop is magnified.
The high dv/dt loop from the SW node is the other main source of radiated noise. Inherently, the dv/dt loop creates an electric field that propagates through space. Parasitic capacitances between the SW node and ground further exacerbate the radiated noise by creating unwanted voltage spikes in the SW waveform. Figure 3-1 shows how both the di/dt and dv/dt signals responsible for the radiated EMI emitted by a buck converter.