SDAA084 April 2026 BQ25856-Q1
Supercapacitors are becoming more and more prevalent as backup systems. Supercapacitors can provide backup power to end equipment such as medical equipment, car doors, and automotive computers. Supercapacitors can also provide supplementary power to servers.
Supercapacitors offer a much longer lifetime and power density compared to battery technologies; however, the impact of aging still needs to be considered. As a supercapacitor ages, the ESR increases and the capacitance decreases. Both of these factors work together to decrease the total usable energy and power in the supercapacitor.
These capacitors need to be reliable and have a long lifetime for their applications. This application note goes over how to quickly measure the capacitance and ESR of a supercapacitor. With the ESR and capacitance information, supercapacitors can be replaced before the capacitor reaches end-of-life (EOL).