SDAA185 February   2026

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
    1. 1.1 NPU Definition and Purpose
    2. 1.2 Key Capabilities
    3. 1.3 Technical Limitations
  5. 2 Development Flow Overview
    1. 2.1 Model Development Phase
    2. 2.2 Model Compilation Phase
    3. 2.3 Application Integration Phase
  6. 3 Example Model Creation (Python)
    1. 3.1 Model Selection Rationale
    2. 3.2 Model Architecture Design
    3. 3.3 Training Details
      1. 3.3.1 Development Environment Setup
      2. 3.3.2 Dataset Generation
      3. 3.3.3 Model Training Configuration
      4. 3.3.4 Quantization-Aware Training Process
  7. 4 Quantization for Embedded Platform
    1. 4.1 Quantization Approaches: QAT versus PTQ
      1. 4.1.1 Post-Training Quantization (PTQ)
      2. 4.1.2 Quantization-Aware Training (QAT)
    2. 4.2 Quantization Frameworks and Wrapper Modules
      1. 4.2.1 Generic Wrappers for CPU Quantization
      2. 4.2.2 TINPU Wrappers for NPU Hardware Acceleration
  8. 5 Validating the Model
    1. 5.1 Two-Phase Training Strategy
      1. 5.1.1 Initial Training Phase
      2. 5.1.2 Fine-Tuning Phase
    2. 5.2 Training Phase Comparison
    3. 5.3 Validation Results and Metrics
  9. 6 Testing the Model
    1. 6.1 Inference Setup and Methodology
      1. 6.1.1 Generic User Testing Approach
    2. 6.2 Testing Results and Visual Analysis
      1. 6.2.1 Visual Performance Assessment
    3. 6.3 Quantitative Performance Metrics
  10. 7 Moving the Model to TI MCU (C2000 – F28P55x) [Beginner Level]
  11. 8 Moving the Model to TI MCU (C2000 – F28P55x) [Developer Level]
    1. 8.1 Compilation Prerequisites
      1. 8.1.1 Required TI Software Components
      2. 8.1.2 Environment Setup Process
    2. 8.2 Configuration File Setup
      1. 8.2.1 Configuration File Structure
        1. 8.2.1.1 Models Requiring Dequantization Flag
      2. 8.2.2 Special Configuration for Regression Models
        1. 8.2.2.1 Output Dequantization Flag
        2. 8.2.2.2 Compiler Constants Modification
        3. 8.2.2.3 Compilation Dictionary Update
    3. 8.3 Compilation Process Flow
      1. 8.3.1 Launching the Compilation
      2. 8.3.2 Compilation Phases
      3. 8.3.3 Common Issues to Watch For
  12. 9 Setting up the MCU Project
    1. 9.1 Creating a CCS Project for NPU Applications
    2. 9.2 Understanding the NPU Interface
      1. 9.2.1 Key Interface Components
      2. 9.2.2 Basic Usage Pattern
  13. 10Testing the Model in the Embedded Environment
    1. 10.1 Visual Performance Assessment
    2. 10.2 Quantitative Performance Metrics
  14. 11NPU Integration in a Real-Time Signal Chain
    1. 11.1 Application Block Diagram
    2. 11.2 Application Code Implementation
    3. 11.3 Hardware Components Utilized
    4. 11.4 Hardware Validation Results
      1. 11.4.1 Input Signal Characteristics
      2. 11.4.2 Neural Network Output Analysis
  15. 12Key Design Decisions and Impact
    1. 12.1 NPU Handling of Numbers
      1. 12.1.1 Integer-Only Architecture
      2. 12.1.2 Working with Negative and Floating-Point Values
    2. 12.2 Supported Neural Network Layers and Constraints
      1. 12.2.1 Supported Layer Types
        1. 12.2.1.1 Convolution Layers
        2. 12.2.1.2 Other Core Layers
        3. 12.2.1.3 Flexibilities
    3. 12.3 Model Complexity and Size Limitations
      1. 12.3.1 Memory Constraints and Model Size
      2. 12.3.2 Optimization Process and Performance Trade-offs
  16. 13Benchmarks
    1. 13.1 Model Performance Comparison
      1. 13.1.1 128 - Neuron Model
      2. 13.1.2 64 - Neuron Model
      3. 13.1.3 16 - Neuron Model
      4. 13.1.4 Reference Benchmark
    2. 13.2 Performance Analysis
      1. 13.2.1 Model Selection Trade-offs
      2. 13.2.2 CPU versus NPU Performance
    3. 13.3 Pipeline Stage Timing Measurements
  17. 14Summary
    1. 14.1 Key Capabilities and Constraints
    2. 14.2 Development Workflow
    3. 14.3 Model Design Considerations
    4. 14.4 Implementation Challenges and Solutions
    5. 14.5 Broader Applications
  18. 15References

CPU versus NPU Performance

The comparison between CPU and NPU execution reveals important insights that should guide implementation decisions:

NPU Advantages for Complex Models: For larger models, the NPU delivers significant performance improvements. The 128-neuron model runs 29.7% faster on the NPU than on the CPU (0.7116ms vs 1.012ms latency), while the 64-neuron model shows a 20.7% latency reduction. This advantage stems from the NPU's specialized architecture for parallel neural network computations.

CPU Advantage for Simple Models: Interestingly, for very small models like the 16-neuron configuration, the CPU actually outperforms the NPU. The CPU achieves 44,643 samples/sec compared to the NPU's 39,557 samples/sec—a 12.9% performance advantage. This counterintuitive result stems from the overhead associated with transferring data to and from the NPU. For the 16-neuron model, the computational workload is so minimal that the CPU can process it directly within its native execution environment, avoiding multiple data transfer steps. With such a small model, the CPU completes the entire inference in a single execution context without the memory transfer penalties that the NPU incurs. Every NPU inference requires setting up DMA transfers, configuring the accelerator, waiting for completion, and retrieving results—operations that collectively consume more time than the actual neural network computation for this lightweight model. Essentially, when the model is this small, the "cost" of using the specialized hardware exceeds its computational benefit.