SDAA262A January   2026  – April 2026 TMS320F28P659DK-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Voltage Stress on Synchronous Rectifier
    2. 1.2 Snubber Circuit Overview
      1. 1.2.1 RC Snubber
      2. 1.2.2 RCD Snubber
      3. 1.2.3 Diode Clamping
      4. 1.2.4 Active Clamping
  5. 2Active Clamping Circuit
    1. 2.1 Different Types of ACL Circuits
      1. 2.1.1 Difference Placement of ACL
      2. 2.1.2 PMOS Type and NMOS Type
    2. 2.2 Hardware Design of ACL Circuit
      1. 2.2.1 Clamping Capacitor
      2. 2.2.2 Power Switches
      3. 2.2.3 Gate Driver
    3. 2.3 Software Design of ACL Circuit
      1. 2.3.1 Turn-on Delay
      2. 2.3.2 Turn-on Duration
  6. 3Summary
  7. 4References
  8. 5Revision History

Clamping Capacitor

The selection of an active clamp capacitor requires careful consideration of multiple design trade-offs involving voltage ripple, transient response characteristics, and overall efficiency. Key design parameters include the capacitance value ( C c l a m p ) and voltage rating. The designer must evaluate the resonant frequency relative to the switching frequency, ensuring the capacitance is sufficiently large to minimize voltage ripple while remaining small enough to facilitate rapid transient response. Additionally, low equivalent series resistance (ESR) capacitor types, such as ceramic capacitors, should be selected to effectively handle resonant currents without generating excessive heat dissipation or voltage overshoot during switching transitions.

  1. Determine Operating Voltages:

    When using ACL, the Vds of secondary SR FETs is clamped to

    Equation 7. V d s _ s r = K × V i n m a x × N s / N p

    in which K is less than 1.5

    Given that the clamping capacitors are connected in parallel with the SR FETs, the voltage across the clamping capacitors is equivalent to the drain-to-source voltage (Vds) of the SR FETs. It is important to note that the clamping capacitors are also subjected to a DC bias voltage equal to:

    Equation 8. V d c _ b i a s = 2 × D × V i n m a x × N s / N p

    in which D is effective duty on transformer primary winding,

    Equation 9. 0 ≤ D < 0.5
  2. Select Resonant Frequency ( f r ): Set f r significantly lower than resonant frequency without ACL f R (for example, f r ≈ 0.1 × f R or less).
    Equation 10. f R = 1 2 × π × Ns Np 2 × L r × 2 × C oss
    Equation 11. f r = 1 2 × π × Ns Np 2 × L r × ( C clamp + 2 × C oss )
  3. Calculate C c l a m p :

    Using the PSFB topology as an example, C c l a m p = 1 / ( ( N s / N p ) 2 × L r × ( 2 π f r ) 2 ) , where L r represents the resonant inductor on the primary side. For other topologies without a discrete resonant inductor, Lr is equivalent to the leakage inductance of the transformer secondary winding. A larger C c l a m p results in a lower resonant frequency f r , which corresponds to reduced voltage ripple across the capacitors. This reduction in capacitor voltage ripple decreases the Vds stress on the SR FETs; however, this also degrades the transient response performance of the converter.

  4. Check I c l a m p :

    Suppose the designed K is 1.1, voltage ripples on capacitors is 0.1 × V i n × N s / N p . Then I c l a m p can be derived from:

    Equation 12. I c l a m p = C c l a m p × ( 0.1 × V i n × N s / N p ) × T d e l a y × f r

    Based on I c l a m p and temperature rise data of capacitors, you can decide the number of capacitors. Notice, I c l a m p is the rms current in clamping time . Find more details about T d e l a y in Section 2.3.1.

  5. Select Capacitor Type:

Use low-ESR ceramic capacitors (such as X7R or C0G etc.) for high-frequency AC performance.

Table 2-1 Summary Checklist for clamping capacitors
Parameter Selection Criteria
V c Must safely handle the peak voltage, typically around V i n + V o u t or 2 V i n (depending on topology), plus margin.
C c l a m p

Larger C c l a m p : Reduces drain voltage ripple (better for efficiency) but slows transient response.

Smaller C c l a m p : Improves transient response but increases ripple.

Trade-off: Find the sweet spot where ripple is acceptable and transients are fast enough (for example, use design tools or datasheet recommendations).

ESRCrucial for managing energy dissipated in the capacitor, especially during fast switching. A low ESR (ceramic caps are great) is preferred to minimize heating and voltage spikes, as the clamp circuit handles resonant currents.