SDAA465 August 2026 LMH13000 , LMH32401
If the photodiode is assumed to be an ideal current source, the output voltage of TIA is given by Equation 3:
For a practical implementation, the photodiode cannot be treated merely as an ideal current source. Instead, the device is more accurately modeled as an ideal current source in parallel with an equivalent shunt resistance, RD, and junction capacitance, CD. The op amp input capacitance also cannot be considered insignificant and must be included as part of CD.
Generally, RD >> RF, RF||RD = RF and the DC gain also becomes unity.
This implies fZ is always lower than fP.
For the system to be stable, the fP must lie inside the open loop curve of op amp.
Figure 4-3 shows three different scenarios for the intersection of the closed-loop response (inverse of the feedback factor) with the open loop gain curve. Instability occurs when the rate of closure of the two curves is 40dB. This happens when the fP falls outside the open loop curve as in case of fP1 and the circuit, in this case, oscillates. If fP lies inside the open loop curve like in the case of fP2, the transimpedance circuit is unconditionally stable, but the stability in this case is traded off for transimpedance bandwidth. The best practice is to place the fP on the open-loop gain curve as shown for fP3.
Since fP is determined by the feedback network, judicious selection of CF. is all that is necessary. This process can be greatly simplified by noting that the high frequency asymptote for the noise gain is determined by capacitance values alone.
For fP to be on AOL curve,
On solving for CF:
Once the photodiode capacitance and op amp GBP are determined, the capacitance value of the feedback capacitor must be selected appropriate as per Equation 9 to Equation 11 to maintain stability.
This result indicates that, for a given op amp and photodiode, transimpedance bandwidth is inversely related to the square root of the feedback resistor. Thus, if bandwidth is a critical requirement, the best approach can be to opt for a moderate transimpedance gain stage followed by a broadband voltage gain stage.