SDAA566 October   2026

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Working Principles
    1. 2.1 Electromagnetic Induction
    2. 2.2 Mathematical Model and Sensitivity
    3. 2.3 Phase Shift: 90° Offset
  6. 3Design Challenges and Workarounds
    1. 3.1 Low Signal Amplitude (μV/A)
    2. 3.2 Sensitivity to Noise
    3. 3.3 Effect of Artificial Load
    4. 3.4 Integration needed
      1. 3.4.1 Integration Theory
      2. 3.4.2 Choosing Integration Frequency: Phase and Gain Margin Versus Number of Decades
    5. 3.5 Stray Magnetic Fields Interference
    6. 3.6 Crosstalk
    7. 3.7 Mechanical Considerations
    8. 3.8 Errors From Non-Ideal Coil Design
  7. 4Summary
  8. 5References

Mathematical Model and Sensitivity

For a Rogowski coil implemented on a PCB, the geometry is constrained by the substrate thickness and the layout area. The induced voltage for a rectangular or cylindrical PCB winding can be modeled by the following relationship:

The Rogowski coil (Vout) is as shown in Equation 1:

Equation 1. B0=μ0Ipsin⁡(ωt)2πR

Where:

  • B0 = magnetic field around a wire generated by the flow of current (Biot-Savart)
  • μ0 = permeability of free space
  • ω = angular frequency = 2πf
  • Ip = primary current
  • R = distance from center of wire to a measuring point

The magnetic flux across the conductive trace is given in Equation 2 as:

Equation 2. Φ=∫abB0×dA

Where:

  • Φ = The magnetic flux across the conductive trace
  • dA = dr × h, which is the rectangular cross section area for element (dr) with PCB height (h)

Where:

  • dr = infinitesimal conductance at a distance R from the center of wire.
  • h = height of PCB

So, the total flux across the conductive trace is as shown in Equation 3:

Equation 3. Φ=μ0Ipsin⁡(ωt)2π×h×ln⁡(ba)

Where:

  • b = outer radius
  • a = inner radius

Proportional voltage to the rate of change of the magnetic flux (\Faraday's law of induction) is as shown in Equation 4. Assuming primary current (Ip) and angular frequency (w).

Equation 4. Vout=N(dΦdt)

Where:

  • N = number of turns

Substituting:

Equation 5. Vout=Nμ0h2π×ln⁡(ba)×dIpsin⁡(ωt)dt

Solving the derivative:

Equation 6. Vout=Nμ0h2π×ωIp×cos⁡(ωt)×ln⁡(ba)
Note: (Vout: Ip) is referred to as sensitivity, typically measured in μV/A.
Note: Mutual inductance is part of Vout.
Equation 7. M=Nμ0h2π×ln⁡(ba)