SFFS234 March 2022 TMP126-Q1
Figure 4-2 shows the TMP126-Q1 pin diagram for the SC70 package. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TMP126-Q1 data sheet.
| Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|
| SCLK | 4 | SCLK stuck low. No SPI communication with device possible. | B |
CS | 1 | CS stuck low. Normal operation. SPI communication still functional. However SPI of device cannot be actively reset anymore by taking CS high and low again. | C |
| GND | 5 | No effect. Normal operation. | D |
| VDD | 6 | Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage may be plausible. | A |
SIO | 3 | SIO stuck low. No SPI communication back to SPI controller possible. Increase in supply current when SIO tries to drive high. Device damage plausible if SIO drives high for extended period of time. | A |
| ALERT | 2 | ALERT stuck low. False thermal limit can be triggered. | B |
| Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|
| SCLK | 4 | State of SCLK input undetermined. No SPI communication with device possible. | B |
CS | 1 | State of CS input undetermined. SPI communication corrupted. | B |
| GND | 5 | Device functionality undetermined. Device may be unpowered or connect to ground internally through alternate pin ESD diode and power up. | B |
| VDD | 6 | Device functionality undetermined. Device unpowered if all external analog and digital pins are held low. Device may power up through internal ESD diodes to VDD if voltages above the device's power-on reset threshold are present on any of the analog or digital pins. | B |
SIO | 3 | State of SIO output undetermined. No SPI communication back to SPI controller possible. | B |
ALERT | 2 | ALERT pin can be left floating or grounded when not used. | B |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|---|
| SCLK | 4 | GND | SPI communication corrupted. No SPI communication with device possible | B |
CS | 1 | ALERT | SPI communication corrupted. Undetermined state of CS. | B |
| GND | 5 | VDD | Device functionality undetermined. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage may be plausible. | A |
| VDD | 6 | GND | Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage may be plausible. | A |
SIO | 3 | ALERT | SPI communication corrupted. No SPI communication with device possible. Increase in supply current possible when SIO tries to drive low while ALERT drives high or vice versa. Device damage plausible if this condition exists for extended period of time. | A |
ALERT | 2 | SIO | Not operational. False thermal limit can be triggered. | D |
| Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|
| SCLK | 4 | SCLK stuck high. No SPI communication with device possible. | B |
CS | 1 | CS stuck high. No SPI communication with device possible | B |
| GND | 5 | Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage may be plausible. | A |
| VDD | 6 | No effect. Normal operation. | D |
SIO | 3 | SIO stuck high. No SPI communication back to SPI controller possible. Increase in supply current when SIO tries to drive low. Device damage plausible if SIO drives low for extended period of time. | A |
| ALERT | 2 | ALERT stuck high. Non-functionable. No thermal limit will be triggered. | B |