SFFS844 April   2024 CD74HCT4051-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the CD74HCT4051-Q1 (SOIC package). The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-6 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality
BNo device damage, but loss of functionality
CNo device damage, but performance degradation
DNo device damage, no impact to functionality or performance

Figure 4-1 shows the CD74HCT4051-Q1 pin diagram for the SOIC package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the CD74HCT4051-Q1data sheet.

GUID-5A0E878F-E9AC-4E81-8CC6-76FC30DEF97C-low.png Figure 4-1 Pin Diagram (SOIC) Package
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
A41Corruption of analog signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, device damage is possible.A
A62Corruption of analog signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, device damage is possible.A
COM OUT/IN A3Corruption of analog signal passed onto the Ax pins. If there is no limiting resistor in the switch path, device damage is possible.A
A74Corruption of analog signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, device damage is possible.A
A55Corruption of analog signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, device damage is possible.A
E6E stuck low. Cannot control switch states.B
VEE7There is no effect; this is normal operation, if the switch path signal voltages are positive. Possible damage to the device if the switch path signal voltages are negative. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible.A
GND8There is no effect; this is normal operation.D
S29Control of the address pin is lost. Cannot control switch.B
S110Control of the address pin is lost. Cannot control switch.B
S011Control of the address pin is lost. Cannot control switch.B
A312Corruption of analog signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, device damage is possible.A
A013Corruption of analog signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, device damage is possible.A
A114Corruption of analog signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, device damage is possible.A
A215Corruption of analog signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, device damage is possible.A
VCC16Device unpowered. Device not functional.A
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
A4 1 Corruption of analog signal passed onto the COM OUT/IN A pin. B
A6 2 Corruption of analog signal passed onto the COM OUT/IN A pin. B
COM OUT/IN A 3 Corruption of analog signal passed onto the Ax pins. B
A7 4 Corruption of analog signal passed onto the COM OUT/IN A pin. B
A5 5 Corruption of analog signal passed onto the COM OUT/IN A pin. B
E 6 Loss of control of E pin. Cannot disable switch. Defaults to switches enabled. B
VEE 7 Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. A
GND 8 Device unpowered. Device not functional. B
S2 9 Control of the address pin is lost. Cannot control switch. B
S1 10 Control of the address pin is lost. Cannot control switch. B
S0 11 Control of the address pin is lost. Cannot control switch. B
A3 12 Corruption of analog signal passed onto the COM OUT/IN A pin. B
A0 13 Corruption of analog signal passed onto the COM OUT/IN A pin. B
A1 14 Corruption of analog signal passed onto the COM OUT/IN A pin. B
A2 15 Corruption of analog signal passed onto the COM OUT/IN A pin. B
VCC 16 Device unpowered. Device not functional. B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted To Description of Potential Failure Effects Failure Effect Class
A4 1 A6 Possible corruption of analog signal passed onto Ax and COM pin. B
A6 2 COM OUT/IN A Possible corruption of analog signal passed onto Ax and COM pin. B
COM OUT/IN A 3 A7 Possible corruption of analog signal passed onto Ax and COM pin. B
A7 A5 Possible corruption of analog signal passed onto Ax and COM pin. B
A5 5 E Possible corruption of the signal passed onto the COM pin. Switch state will be undefined. B
E 6 VEE

Possible damage to device if the signal voltage is negative. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible.

A
VEE 7

GND

Possible damage to device if the signal voltage is negative. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. A
GND 8 S2 Not considered; corner pin. D
S2 9 S1 Control of the switch state is lost. B
S1 10 S0 Control of the switch state is lost. B
S0 11 A3 Possible corruption of the signal passed onto the Ax and COM pin. Control of the switch state is lost. B
A3 12 A0 Possible corruption of the signal passed onto the Ax and COM pin. B
A0 13 A1 Possible corruption of the signal passed onto the Ax and COM pin. B
A1 14 A2 Possible corruption of the signal passed onto the Ax and COM pin. B
A2 15 VCC Corruption of the signal passed onto the Ax pin. If there is no limiting resistor in the switch path, then device damage is possible. A
VCC 16 A4 Not considered, corner pin. D
Table 4-5 Pin FMA for Device Pins Short-Circuited to Supply
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
A4 1 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
A6 2 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
COM OUT/IN A 3 Corruption of the signal passed onto the Ax pins. If there is no limiting resistor in the switch path, then device damage is possible. A
A7 4 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
A5 5 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
E 6 E stuck high. Can no longer enable the device. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. A
VEE 7 Device is unpowered. Device is not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. A
GND 8 Device is unpowered. Device is not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. A
S2 9 Address stuck high. Cannot control switch states. B
S1 10 Address stuck high. Cannot control switch states. B
S0 11 Address stuck high. Cannot control switch states. B
A3 12 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
A0 13 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
A1 14 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
A2 15 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
VCC 16 No effect. Normal operation. D
Table 4-6 Pin FMA for Device Pins Short-Circuited to VEE
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
A4 1 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
A6 2 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
COM OUT/IN A 3 Corruption of the signal passed onto the Ax pins. If there is no limiting resistor in the switch path, then device damage is possible. A
A7 4 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
A5 5 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
E 6 Possible damage to the device if signal voltage is negative. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. A
VEE 7 No effect. Normal operation. D
GND 8 Possible damage to the device if signal voltage is negative. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. A
S2 9 Possible damage to the device if signal voltage is negative. Cannot control switch states. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. A
S1 10 Possible damage to the device if signal voltage is negative. Cannot control switch states. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. A
S0 11 Possible damage to the device if signal voltage is negative. Cannot control switch states. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. A
A3 12 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
A0 13 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
A1 14 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
A2 15 Corruption of the signal passed onto the COM OUT/IN A pin. If there is no limiting resistor in the switch path, then device damage is possible. A
VCC 16 Possible damage to the device if signal voltage is negative. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. A