SLAA701B October 2016 – June 2026 TAS5342A , TAS5342LA , TAS5352 , TAS5630B , TPA3220 , TPA3221 , TPA3251 , TPA3255 , TPA3255-Q1
Capacitor manufacturers provide a maximum temperature rise or operating temperature to prevent overheating of the capacitor. For convenience, most manufacturers provide AC voltage or current limits that correspond to the maximum temperature limit. The maximum rms voltage and current are typically provided in a graph versus frequency. The AC voltage and current limits provide a way to limit power dissipation and prevent capacitor overheating.
For audio LC filter applications, the losses due to AC voltage and current are a result of the ripple voltage from the inductor charge and discharge cycles. The charge and discharge cycle frequency occurs at the class-D switching frequency.
To estimate power losses and temperature rise, first use the ripple current calculation in Equation 12 and then use the following equations for power losses in the capacitor.
It is always good practice to calculate the temperature rise due to AC voltage and current through the capacitor using ESR or dissipation factor.
| ESR | Dissipation Factor | ||||||||
|---|---|---|---|---|---|---|---|---|---|
Equation 16. ![]() | Equation 17. ![]() | ||||||||
| Parameter | Description | Units | Parameter | Description | Units | ||||
| Plosses | Power Dissipation in Capacitor | W | Plosses | Power Dissipation in Capacitor | W | ||||
| Vripple | RMS Ripple Voltage | VRMS | Vripple | RMS Ripple Voltage | VRMS | ||||
| Iripple | RMS Ripple Current | IRMS | f | Ripple Frequency | Hz | ||||
| ESR | Equivalent series resistance | Ω | C | Capacitance | F | ||||
| tan δ | Dissipation Factor | - | |||||||
Note: Use the ESR value at the same frequency as the ripple current. | Note: Use the dissipation factor value at the same frequency as the ripple current. | ||||||||
Using the power losses calculated in Equation 16 and Equation 17, the capacitor temperature due to self-heating can be calculated using the heat coefficient in the capacitor data sheet. Typically, there is a heat coefficient represented as the ratio of temperature rise to the power dissipated in watts. The thermal coefficient typically takes into account the capacitor size and surface area.
Equation 18 is read, “For every 1 W of power dissipated, there is a temperature change of Δ°C.”
Audio Importance
Rated AC voltage or current is very important for high-power audio applications, because of high ripple currents passing through the capacitor. Be sure to verify the capability of the chosen capacitor in the data sheet and measure temperature under worst-case conditions.