SLAA877 December   2018 MSP430FR2633

 

  1.   Capacitive Touch Gesture Software and Tuning
    1.     Trademarks
    2. 1 Introduction
    3. 2 Gestures
      1. 2.1 Theory of Operation
      2. 2.2 Sensor Gesture Processing
      3. 2.3 Gesture Software Overview
        1. 2.3.1 Slider Gesture
        2. 2.3.2 Wheel Gesture
        3. 2.3.3 Button Gesture
        4. 2.3.4 Sensor Handlers
        5. 2.3.5 How to Add Gestures to the CapTIvate Framework
    4. 3 Tuning
      1. 3.1 CapTIvate Design Center
        1. 3.1.1 Enabling Gesture Sensor Output
        2. 3.1.2 CDC Plot Channel Assignments
      2. 3.2 Tuning Process
        1. 3.2.1 Tap
        2. 3.2.2 Double Tap
        3. 3.2.3 Swipe
        4. 3.2.4 Slide
    5. 4 Example Demonstration Software Installation
      1. 4.1 Project Directories
      2. 4.2 Import the Project Into CCS

Tuning

To achieve a good user experience with gesture-based capacitive touch interfaces, a gesture's responsiveness should be adjusted to meet the application's user interface requirements. This is an iterative process requiring the adjustment of the gesture timing and distance parameters. You are encouraged to experiment with the timing and motion parameters to understand the relationship between the settings and the sensor's responsiveness.