SLAA954 August 2020 – MONTH TAS2563
Define the Pass/Fail Limits of each parameter based on the speaker datasheet tolerance or on the application requirement. Select “Next” to generate the binary, ftcfg, cfg, and header files
Figure 2-2 FTC Pass/Fail Limits. In some cases, if the speaker parameter tolerances are not defined in the speaker datasheet, it is recommended to use Re variation as the limits for Re, and 6-Sigma deviation of Re variation as the variation limits for the rest of the speaker parameters