SLAAEE3 july 2023 MSPM0L1306 , MSPM0L1306
For this mode, the battery running data is input from the GUI. It enables you to run the real test case or evaluate the MSPM0 Gauge with only a launchpad. This method can remove the need of hardware, increase algorithm running frequency and have no limit to the length of battery running data.
To realize this method, first you need to connect the UART COM port and load the MCUData runfile in MCU COM Tool. After clicking the data transmit button, you need to wait until the port status changes to “Start transmition!”, shown in Figure 4-13. The data load time and excel save time will be long if the file is very large. It would be 5~10 minutes.
You will receive the battery running data from MCU. The most benefit of the method is that you can load the battery running data over and over again to improve the algorithm and parameter setting.