SLAAEF7 November 2023 DAC81401
Design Goals
| DAC VOUT | Gain Stage | External Supply | ||||
|---|---|---|---|---|---|---|
| Range | MIN | MAX | MIN | MAX | HV+ | HV– |
| 0 V–20 V | 0 V | 20 V | 0 V | 80 V | 0 V | 82 V |
| ±10 V | –10 V | +10 V | –40 V | +40 V | –41 V | +41 V |
Objective: Design a high-voltage gain (4 ×) stage in a closed loop system for the DAC81401.
Design Description
This high-voltage gain stage design circuit for the DAC81401 is capable of providing output voltage ±40 V or 0 V to 80 V. This system design consists of four blocks as listed below and shown in High-Voltage Gain Stage Circuit Block Diagram.
The DAC81401 output voltage is amplified by the gain stage by a factor of 4. The gain stage output is attenuated by the attenuation stage by a factor of 4. This attenuated output voltage is buffered and connected to the VSENSEP pin of the DAC81401 to close the loop.
Key Components
DAC81401 Output Stage
The DAC81401 output (VOUT) is capable of providing from –20 V to +40 V. However, some applications (test and measurement, factory automation and control) requires even higher voltages. The high-voltage gain stage design is useful in these applications.
VOUT is expressed by using the next two equations.
For unipolar mode:
For bipolar mode:
where:
Compensation Capacitor
A 470-pF compensation capacitor is optional and the CCOMP pin can be left floating. This compensation capacitor is only needed if the load capacitor at the DAC81401 VOUT node is greater than 2 nF.
Adding the compensation capacitor increases the output settling time and slows the output voltage transient.
Gain Stage
The gain stage amplifies the DAC output voltage by 4 ×. This gain stage utilizes the OPA593 (U1) which supports an output voltage range of 85 V for single supply or ±42.5 V for bipolar supply. At the gain stage output (VOUT_HV), 0 V to 80 V or ±40 V can be obtained by programming the DAC output range to, 0 V to 20 V or ±10 V, respectively. For a given gain stage output (VOUT_HV), the DAC output can be calculated with the next two equations.
For unipolar mode:
For bipolar mode:
And for a given DC code, the gain stage output voltage can be calculated with the following equations.
For unipolar mode:
For bipolar mode:
Attenuation Stage
To avoid any unintended voltage drop due to load current (IR drop), VOUT and VSENSEP are connected close to the load, and the voltage value for the VSENSEP and VOUT is same. To remove the IR drop, the gain stage output voltage is – first buffered (U2) and then attenuated by a factor of 4 with resistor divider R5 and R6.
Buffer Stage
The VSENSEP pin has an input impedance of about 50 kΩ and the resistor divider voltage cannot be connected directly or loading causes a voltage error. This voltage output is first buffered (U3) and then connected to the VSENSEP pin of DAC81401 to close the internal feedback loop with VOUT.
Design Accuracy
The gain stage output has an error contributed by mostly from:
The calculated error contributions from U1, R1, and R3 show that the final gain stage output is just as accurate as the DAC81401.
Measurement Result
Integral nonlinearity (INL) and total unadjusted error (TUE) at the gain stage output were measured for different output voltage ranges. The INL and TUE plots from the next four images are measured for linear codes spans from code 512 to code 65024.
The DAC81401 voltage output range and corresponding gain stage voltage output range are listed in the following table.
| DAC81401 VOUT Range | Gain Stage Voltage Range |
|---|---|
| 0 V–5 V | 0 V–20 V |
| 0 V–10 V | 0 V–40 V |
| 0 V–20 V | 0 V–80 V |
| ±5 V | ±20 V |
| ±10 V | ±40 V |
Power Supply Requirement
An external high-voltage power supply is needed for the OPA593 in the gain stage (U1) and the attenuation stage (U2). The supplies also need to meet the headroom and footroom requirements as per the OPA593 85-V, 250-mA Output Current, Precision, Power Op Amp data sheet. These external power supplies need to be provided from a high-voltage supply source. Typical values used for HV+ and HV– are +41 V and −41 V or 81 V and 0 V, respectively.
Where VOUT_HV is output of the gain stage (U1) in the block diagram shown in High-Voltage Gain Stage Circuit Block Diagram.
Set the DAC81401 power supply as recommended by the DACx1401 Single-Channel, 16-Bit and 12-Bit, High-Voltage Output DACs With Precision Internal Reference data sheet. AVDD and AVSS of the DAC81401 can be used for the V+ and V– power supply of the buffer stage operational amplifier (U3).
Overvoltage Stress (OVS) Protection Design
If the OPA593 (U1 and U2) output pins are exposed to industrial transient testing without external protection components, the internal diode structures of the DAC81401 becomes forward biased and conducts current. If the conducted current is large, as is common in high-voltage industrial transient tests, the structures can get permanently damaged and impact the device functionality.
The gain stage output and attenuation stage input includes an external electrical overstress protection circuit for short-circuit events. Protection is achieved by using the transient voltage suppressor (TVS) diodes D3 and D6 and clamp-to-rail diodes D1, D2, D4, and D5.
The combined protection from the TVS and clamp-to-rail diodes limits the current flowing into the device internal diode structures to prevent permanent damage. Considering R1 = 10 Ω and diode forward biased voltage is 0.7 V, the peak current entering to the device (U1 and U2) is 80 mA when the Schottky diode clamps VOUT to ±1.5 V from the rail. It is also important to connect the TVS diodes D3 and D6 to the gain stage output and attenuation stage input nodes to provide a discharge path for the energy sent to these nodes through diodes D3, D6, and the internal diode structures. R1 helps to limit the peak transient current or steady state current in case of incorrect bias voltage.
Pseudocode Example
The following pseudocode sequence example:
//Write these SPI commands after the device power supply is power configured
//Device power up
WRITE 0x0A04 to SPI_CONFIG register (0x03)
//Internal reference power up
WRITE 0x0000 to GEN_CONFIG register (0x04)
//DAC channel power up
WRITE 0xFFFE to DAC_PWDWN register (0x09)
//Configure the gain stage voltage output, default voltage range is 0 V to 20 V
//For 20 V span
WRITE 0x0000 to DACRANGE register (0x0A)
//For 5 V
WRITE 0x3FFF to DAC register (0x10)
//For 10 V
WRITE 0x7FFF to DAC register (0x10)
//For 15 V
WRITE 0xBFFF to DAC register (0x10)
//For 20 V
WRITE 0xFFFF to DAC register (0x10)Design Featured Devices
| Device | Key Features | Link |
|---|---|---|
| OPA593 | 85-V, Low offset, Low noise, 10 MHz, 250 mA output current precision operational Amplifier | OPA593 |
| OPA189 | 36-V, Low offset, Low drift, Low noise, 14 MHz precision operational amplifier | OPA189 |
Design References
See the Analog Engineer's Circuit Cookbooks for TI's comprehensive circuit library.
Additional Resources
For direct support from TI Engineers, use the E2E™ community: