SLAAET4A April 2025 – October 2026 MSPM0G3506 , MSPM0G3507 , MSPM0G3518 , MSPM0G3519
This document begins with an overview of the CAN bus and the features of MCAN module integrated in the MSPM0 MCU. The application note details how to use Sysconfig to configure the CAN module, so that users can adjust related parameters to meet application requirements. This document briefly describes the demo example related to MCAN module provided in the MSPM0 SDK. Also, based on production experience, introduce some common use case with user defined example code. Finally, some common debugging issues and relevant debugging suggestions from the software and hardware aspects are introduced.