SLAU533D September 2013 – April 2017
It is often beneficial to evaluate the LaunchPad development kit with an external power source (see Figure 18). To see accurate system power when performing this action, it is best to disconnect all jumpers in the isolation block, so that additional power is not consumed by back-powering the emulation MCU through its I/Os. The 5-V jumper can be left populated for proper USB operation and to allow for 5 V to the target side.
Figure 18. Power Block Diagram for External 3.3-V Power Source Step 2 requires that emulation is not possible if you are using an external power source at a voltage other than 3.3 V. But USB can be used under these conditions, because there is no connection between the USB module VBUS and VUSB rails and the DVCC and AVCC rails used by the rest of the F5529.