SLAU646F September 2015 – June 2020
For MSP430X devices in the large memory model, pointers and size_t are 20 bits in
size. To handle this, GCC defines the __int20 type, which uses 20
bits of space in registers, and 32 bits of space in memory.
This type is built into the compiler, so it can be used like any other type in source
code. Using unsigned __int20 designates the unsigned version of the
type.
The __int20 type is not part of the ISO C specification, so using this type in any
program compiled with flags that check for standards compliance may cause a warning
or error to be emitted. A variation of the type that will not trigger these
standards compliance messages is defined as __int20__ (using a
trailing double underscore).