SLAU927 March 2024 MSPM0G3507
Configure the system parameters using the System Configuration page in the GUI as shown below. If the parameters are already programmed in the firmware for a given system, the GUI page displays the default programmed values upon pressing READ ALL REGS. These parameters to be updated accordingly from the below steps.