SLAZ755D May   2024  – July 2026 MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4.   4
  5. 1Functional Advisories
  6. 2Preprogrammed Software Advisories
  7. 3Debug Only Advisories
  8. 4Fixed by Compiler Advisories
  9. 5Device Nomenclature
    1. 5.1 Device Symbolization and Revision Identification
  10. 6Advisory Descriptions
    1. 6.1  ADC_ERR_05
    2. 6.2  ADC_ERR_06
    3. 6.3  AES_ERR_01
    4. 6.4  COMP_ERR_03
    5. 6.5  COMP_ERR_04
    6. 6.6  CPU_ERR_01
    7. 6.7  CPU_ERR_02
    8. 6.8  CPU_ERR_03
    9. 6.9  CPU_ERR_04
    10. 6.10 CRC/CRCP_ERR_01
    11. 6.11 FLASH_ERR_04
    12. 6.12 FLASH_ERR_05
    13. 6.13 FLASH_ERR_08
    14. 6.14 FLASH_ERR_09
    15. 6.15 GPIO_ERR_03
    16. 6.16 GPIO_ERR_04
    17. 6.17 GPIO_ERR_06
    18. 6.18 I2C_ERR_01
    19. 6.19 I2C_ERR_03
    20. 6.20 I2C_ERR_04
    21. 6.21 I2C_ERR_05
    22. 6.22 I2C_ERR_06
    23. 6.23 I2C_ERR_07
    24. 6.24 I2C_ERR_08
    25. 6.25 I2C_ERR_09
    26. 6.26 I2C_ERR_10
    27. 6.27 I2C_ERR_13
    28. 6.28 I2C_ERR_15
    29. 6.29 KEYSTORE_ERR_01
    30. 6.30 LCD_ERR_01
    31. 6.31 LFSS_ERR_01
    32. 6.32 LFSS_ERR_02
    33. 6.33 LFSS_ERR_03
    34. 6.34 LFXT_ERR_01
    35. 6.35 LFXT_ERR_02
    36. 6.36 PMCU_ERR_08
    37. 6.37 PMCU_ERR_09
    38. 6.38 PMCU_ERR_10
    39. 6.39 PMCU_ERR_12
    40. 6.40 RST_ERR_01
    41. 6.41 RST_ERR_02
    42. 6.42 RTC_A_ERR_02
    43. 6.43 SPI_ERR_03
    44. 6.44 SPI_ERR_04
    45. 6.45 SPI_ERR_05
    46. 6.46 SPI_ERR_06
    47. 6.47 SPI_ERR_07
    48. 6.48 SPI_ERR_10
    49. 6.49 SRAM_ERR_01
    50. 6.50 SYSCTL_ERR_01
    51. 6.51 SYSCTL_ERR_02
    52. 6.52 SYSCTL_ERR_03
    53. 6.53 SYSCTL_ERR_04
    54. 6.54 SYSCTL_ERR_05
    55. 6.55 SYSCTL_ERR_06
    56. 6.56 SYSOSC_ERR_01
    57. 6.57 SYSOSC_ERR_02
    58. 6.58 SYSOSC_ERR_04
    59. 6.59 SYSOSC_ERR_05
    60. 6.60 SYSOSC_ERR_06
    61. 6.61 TAMPERIO_ERR_01
    62. 6.62 TIMER_ERR_01
    63. 6.63 TIMER_ERR_04
    64. 6.64 TIMER_ERR_06
    65. 6.65 TIMER_ERR_07
    66. 6.66 UART_ERR_01
    67. 6.67 UART_ERR_02
    68. 6.68 UART_ERR_03
    69. 6.69 UART_ERR_04
    70. 6.70 UART_ERR_05
    71. 6.71 UART_ERR_06
    72. 6.72 UART_ERR_07
    73. 6.73 UART_ERR_08
    74. 6.74 UART_ERR_09
    75. 6.75 UART_ERR_10
    76. 6.76 UART_ERR_11
  11. 7Revision History

Device Nomenclature

To designate the stages in the product development cycle, TI assigns prefixes to the part numbers of all MSP MCU devices. Each MSP MCU commercial family member has one of two prefixes: MSP or XMS. These prefixes represent evolutionary stages of product development from engineering prototypes (XMS) through fully qualified production devices (MSP).

XMS – Experimental device that is not necessarily representative of the final device's electrical specifications

MSP – Fully qualified production device

Support tool naming prefixes:

X: Development-support product that has not yet completed Texas Instruments internal qualification testing.

null: Fully-qualified development-support product.

XMS devices and X development-support tools are shipped against the following disclaimer:

"Developmental product is intended for internal evaluation purposes."

MSP devices have been characterized fully, and the quality and reliability of the device have been demonstrated fully. TI's standard warranty applies.

Predictions show that prototype devices (XMS) have a greater failure rate than the standard production devices. TI recommends that these devices not be used in any production system because their expected end-use failure rate still is undefined. Only qualified production devices are to be used.

TI device nomenclature also includes a suffix with the device family name. This suffix indicates the temperature range, package type, and distribution format.