SLDU028A January 2018 – March 2020
After connecting the USB cable to the EVM and launching the GUI, click the Re-Initialize USB2ANY button to sync the GUI with the EVM. If the GUI is successfully synchronized with the EVM, the GUI connection status field on the bottom right of the GUI turns green and HARDWARE CONNECTED is displayed (see Figure 4). The GUI is now connected to the EVM. If the GUI is not synchronized correctly, DEMO MODE is displayed with a grey background.