SLLA454A April 2019 – August 2024 TUSB211A , TUSB212 , TUSB213 , TUSB214 , TUSB215 , TUSB216 , TUSB217A
With all those different potential causes for signal degradation of a USB 2,0 signal, the question of whether to use a USB 2.0 redriver and where to use it becomes an important one. Often, designers hesitate under the assumption that adding a redriver can require an extensive rework, and if the redriver does not work, this can require another rework to correct the changes made. Thankfully, a USB 2.0 redriver is actually one of the easier redrivers to implement. USB 2.0 redriver come in a small form factor and flow through trace routing can be used in the board design. Figure 3-1 shows the flow-through design.
Figure 3-1 Flow-Through DesignEssentially, this flow-through trace routing means that a USB 2.0 redriver does not need to directly integrate a signal through the device as an input to be boosted and then output back onto a trace, but can instead passively monitor the signal as it passes under the redriver. That way, the PCB trace of a board does not need to be extensively reworked to incorporate a USB 2.0 redriver, and if the redriver is not necessary, the redriver can be removed with no worries about whether the trace can be affected or not. Additionally, a USB 2.0 redriver comes in a smaller form-factor, causing it to take up a minimal amount of space in a signal, and is easy to setup, with 1-2 configuration pins at most.