The eZ-FET Debug Probe on the
MSP430FR2355 LaunchPad uses a SPI-by-Wire JTAG interface to program the MSP430FR2355
MCU on the MCT8329EVM. Consult the MSP430 LaunchPad Development Kits for MSP430 LaunchPads
that include an onboard eZ-FET Debug Probe.
- Remove the GND, 3V3, SBWTDIO, and
SBWTCK jumpers from the MSP430 LaunchPad.
- Connect the top pins on the
eZ-FET side of the LaunchPad of the GND, 3V3, SBWTCK, and SBWTDIO signals to
their respective pins on J7 of the MCT8329EVM as shown in Table 7-1 and Figure 7-2.
- Connect a micro-USB cable to the
MSP430 LaunchPad and the PC.
- Click on the Build Project icon
or Ctrl + B to verify that the project builds successfully. Accept any
updates if needed from the Console.
- Click on Debug Project to set up
a debug session and press the Play button to run the code.
- Stop the debug session, close
Code Composer Studio, disconnect the SPI-by-Wire jumpers, and unplug the
micro-USB cable from the MSP430 LaunchPad.
Table 7-1 SPY-BI-Wire Connections Needed
to Program MSP430FR2355
| MSP430 LaunchPad (eZ-FET
Debug Probe Side) (J101) |
MCT8329EVM 4-pin
SPI-by-Wire Header (J7) |
| GND |
GND |
| 3V3 |
3.3 V |
| SBWTDIO |
SBWTDIO |
| SBWTCK |
SBWTCK |