SLOS197B August 1997 – July 2025 TLV2721
PRODUCTION DATA
The TLV2721 is designed to drive larger capacitive loads than most CMOS operational amplifiers. Figure 5-27 and Figure 5-28 illustrate an ability to drive loads greater than 100pF while maintaining good gain and phase margins (Rnull = 0Ω).
A small series resistor (Rnull) at the output of the device (Figure 7-1) improves the gain and phase margins when driving large capacitive loads. Figure 5-27 and Figure 5-28 show the effects of adding series resistances of 100Ω, 200Ω, 500Ω, and 1kΩ. The addition of this series resistor has two effects: the first effect is that the resistor adds a zero to the transfer function and the second effect is that the resistor reduces the frequency of the pole associated with the output load in the transfer function.
The zero introduced to the transfer function is equal to the series resistance times the load capacitance. To calculate the approximate improvement in phase margin, use the following equation:
Where:
∆φm1 = Improvement in phase margin
UGBW = Unity-gain bandwidth frequency
Rnull = Output series resistance
CL = Load capacitance
The unity-gain bandwidth (UGBW) frequency decreases as the capacitive load increases. To use Equation 1, approximate UGBW for the given capacitive load in Figure 7-1.
The TLV2721 is designed to provide better sinking and sourcing output currents than earlier CMOS rail-to-rail output devices. This device is specified to sink 500µA and source 1mA at VDD = 5V at a maximum quiescent IDD of 200µA. This provides a greater than 80% power efficiency.
When driving heavy dc loads, such as 2kΩ, the positive edge under slewing conditions can experience some distortion; see also Figure 5-22. This condition is affected by three factors: