SLOU559 April   2023

 

  1.   Abstract
  2.   Trademarks
  3. 1 Introduction
    1. 1.1 DRV8845 Quad H-bridge motor driver
    2. 1.2 DRV8849 Dual Stepper driver
  4. 2 Jumpers Table and Setup
  5. 3 Software Setup
  6. 4 Cloud-based GUI
  7. 5 Local Installation
  8. 6 Hardware Setup
  9. 7 Launching the DRV884x-EVM-GUI Application
  10. 8 GUI Operations DRV8845
  11. 9 GUI Operations DRV8849
  12. 10Updating Firmware
  13. 11Revision History

Software Setup

  1. Install the TI MSP430 USB driver from MSP430 FET Drivers.

    1. Click on the driver download link highlighted in the image below.

    2. Please login with your myTI credentials when prompted and provide the requested information. The approval to access the download is automatic and immediate as long as the U.S. Government export approval requirements are complied with

      GUID-20230324-SS0I-7CPW-5THC-QLQJQH8T6LP9-low.pngFigure 3-1 FET Drivers Product Download List

    3. Click on the download button to download the installer to your PC.

    4. Double click on the downloaded zip file and run the installer by double clicking on the “.exe” file.

      1. Complete the installation.

      2. The required USB drivers to use the EVM are installed in your PC.

      3. Please follow proper safety precautions working with sensitive electronics as well as high voltage and high current hardware.

      4. Power sequencing: The USB cable must be plugged in first between the EVM and the computer. Then turn on the power supply to the EVM. Powering the EVM external bench supply before connecting the USB cable can cause the USB device to not start up properly and result with driver error.

      5. Setup the bench supply to 12 V with current limit set to appropriate requirements of the motor.

      6. The computer then recognizes the USB device is connected and enumerates as serial ports in the system as shown below. The COMxx numbers can vary according to your system.

      7. Login to https://dev.ti.com/gallery/ using your myTI login credentials. Please note the GUI composer login looks for a very specific username match including case input at the time of sign up.