SLUAAG5 March   2022 TPS62933

 

  1.   Trademarks
  2. 1Introduction
  3. 2Cff in High-Output Voltage Internally Compensated PCM Buck Converter
  4. 3Effects of Cff on the Loop
  5. 4Method for Selecting Cff
  6. 5Experimental Verification for TPS62933
  7. 6Summary
  8. 7References
  9.   A Validation Results for the Proposed Method

Effects of Cff on the Loop

The Optimizing Transient Response of Internally Compensated dc-dc Converters With Feedforward Capacitor application report details the effects of adding a feedforward capacitor in the feedback divider. Figure 3-1 shows feedback divider including Cff.

Figure 3-1 Scheme of Feedback Divider Including Feedforward Capacitor

Cff introduces a pair of zero and pole in the converter loop. The frequency of the introduced zero and pole are:

Equation 5.
Equation 6.

Figure 3-2 shows the effects of the zero and pole introduced by Cff.

Figure 3-2 Bode Plot of Feedback Divider Transfer Function Including Cff

Cff has both effects on the loop gain and phase. The loop gain is increased to enlarge bandwidth which benefits transient response, and the phase is also boosted to increase the phase margin for system stability.

In application notes such as Optimizing Transient Response of Internally Compensated dc-dc Converters With Feedforward Capacitor, some methods have been proposed to use Cff for phase margin enhancement. But in those methods, the bode plot results without Cff are always needed to get the recommended Cff value. The Cff selecting method is more applicable in the solution validation process but not in the application design process.

A new method to choose Cff is proposed in this application report. The bode plot results without Cff are not needed to get the recommended Cff value in this method, which makes it more applicable in TPS62933 application design.