SLUAB17 February   2025 AFE7950-SP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Sensor Technology in Satellites
  5. 2Active Sensing Payloads for Satellites
  6. 3Passive sensing systems for satellites
  7. 4Conclusion

Sensor Technology in Satellites

The types of sensing payloads (also known as “sensing instruments”) used in satellites for measurement can be broken down into two categories:

  • Active sensors generate their own illumination in the form of light or electromagnetic waves, similar to using a flash on a camera. The synthetic aperture radar (SAR) aboard the satellite launched in the joint NASA-Indian Space Research Organization (NISAR) ISRO mission in 2025 is an example of an active sensor.
  • Passive sensors sense illumination from other sources, similar to taking a picture outside where the sun is providing the light. An example of a passive sensor is a multispectral imager such as those used on the Sentinel 2 mission from the European Space Agency (ESA).