SLUSCU0L march 2018 – august 2023 BQ77915
PRODUCTION DATA
When the CHG driver is off, CHG is pulled to VSS, the PACK– terminal can be pulled up to the PACK+ level when a load is connected. This can put the gate-source voltage above the absolute max of the MOSFET rating. Thus, it is common to place a Zener diode across the CHG FET’s gate source to protect the CHG FET. Additional components are added when a Zener is used to limit current going into the CHG pin, as well as reducing the impact on rise time. See Figure 10-4 for details.
Figure 10-4 Protecting the CHG FET from High Voltage on PACK–
Figure 10-5 Optional Components
Combining and Protections