SLUSDF8F June 2019 – February 2025 BQ25618 , BQ25619
PRODUCTION DATA
The BATFET functions as a load switch between the battery and system when an input source is not plugged in. When BATFET_RST_EN = 1 and BATFET_DIS = 0, the BATFET full system reset function is enabled. By changing the state of BATFET from on to off, systems connected to SYS can be effectively forced to have a power-on-reset. After the reset is complete, the device is in the POR state, and all registers are in POR default settings. The QON pin supports a push-button interface to reset system power without the host by changing the state of BATFET. Internally, it is pulled up to the VQON voltage through a 200-kΩ resistor.
When the QON pin is driven to logic low for tQON_RST, the BATFET reset process starts. The BATFET is turned off for tBATFET_RST and then it is re-enabled to reset system power. This function can be disabled by setting the BATFET_RST_EN bit to 0.
The BATFET full system reset functions either with or without an adapter present. If BATFET_RST_WVBUS = 1, the system reset function starts after tQON_RST when the QON pin is pushed to LOW. Once the reset process starts, the device first goes into HIZ mode to turn off the converter, and then power cycles BATFET. If BATFET_RST_WVBUS = 0, the system reset function does not start until tQON_RST after the QON pin is pushed to LOW and the adapter is removed.
After the BATFET full system reset is complete, the device powers up again if EN_HIZ is not set to 1 before the system reset.
Figure 7-6 QON Timing