SLUSF07 December 2024 TPS4813-Q1
PRODUCTION DATA
For selecting the MOSFET Q1 and Q2, important electrical parameters are the maximum continuous drain current ID, the maximum drain-to-source voltage VDS(MAX), the maximum drain-to-source voltage VGS(MAX), and the drain-to-source ON resistance RDSON.
The maximum continuous drain current, ID, rating must exceed the maximum continuous load current.
The maximum drain-to-source voltage, VDS(MAX), must be high enough to withstand the highest voltage seen in the application. Considering 70V as the maximum application voltage due to load dump, MOSFETs with VDS voltage rating of 80V is chosen for this application.
The maximum VGS TPS48130-Q1 can drive is 11V, so a MOSFET with 15V minimum VGS rating must be selected.
To reduce the MOSFET conduction losses, an appropriate RDS(ON) is preferred.
Based on the design requirements, two of IAUS200N08S5N023 are selected and its ratings are:
TI recommends to make sure that the short-circuit conditions such max VIN and ISC are within SOA of selected FETs (Q1 and Q2) for > tSC timing.
The internal charge pump charges the external bootstrap capacitor (connected between BST and SRC pins) with approximately 345μA. Use the following equation to calculate the minimum required value of the bootstrap capacitor for driving two parallel IAUS200N08S5N023 MOSFETs.
Choose closest available standard value: 220nF, 10%.
The RISCP sets the short-circuit protection threshold, whose value can be calculated using following equation:
To set 100A as short-circuit protection threshold, RISCP value is calculated to be 48kΩ for two FETs in parallel.
Choose the closest available standard value: 48.1kΩ, 1%.
For the design example under discussion, overcurrent transients are allowed for 20μs duration. This blanking interval, tSC (or circuit breaker interval, TCB) can be set by selecting appropriate capacitor CTMR from TMR pin to ground. The value of CTMR to set 20μs for tSC can be calculated using following equation:
Choose closest available standard value: 1.5nF, 10%.
TMR pin can be left floating for fast response of tSC <10μs.
During normal operation, the resistor RBYPASS along with bypass FET RDSON is used to set load wakeup current threshold.
For selecting the MOSFET Q3, important electrical parameters are the maximum continuous drain current ID, the maximum drain-to-source voltage VDS(MAX), the maximum drain-to-source voltage VGS(MAX), and the drain-to-source ON resistance RDSON.
Based on the design requirements, SQS182ELNW-T1 is selected and its ratings are:
The recommended range of the short-circuit threshold voltage which is same as load wakeup threshold, V(SCP/LWU), extends from 20mV to 500 mV. Values near the low threshold of 20mV can be affected by the system noise. Values near the upper threshold of 500mV would result in high short-circuit current threshold. To minimize both the concerns, 50mV is selected as the short-circuit or load wakeup threshold voltage.
The V(SCP/LWU) value can also be calculated based on selected RISCP resistor by following equation:
RBYPASS resistor value can be selected using below equation:
To set 50 mA as load wakeup threshold, RBYPASS value is calculated to be ~2.3Ω.
The average power rating of the bypass resistor can be calculated by following equation:
The average power dissipation of RBYPASS is calculated to be ~5.75mW
The peak power dissipation in the bypass resistor is given by following equation:
The peak power dissipation of RBYPASS is calculated to be ~1565W
The peak power dissipation time for power-up with short into LPM can be calculated based on following equation:
where,
V(G2_GOOD) is internal threshold with 7V (typical) value,
I(G2) is 165μA (typical),
VGS(th) is gate to source voltage and CISS is effective input capacitance of selected bypass FET.
Based on Equation 28, TPULSE is calculated to be ~60μs.
Two 4.7Ω, 1.5W, 1% CRCW25124R70FKEGHP resistor are used in parallel to support both average and peak power dissipation for >TPULSE time calculated in Equation 28.
TI suggests the designer to share the entire power dissipation profile of bypass resistor with the resistor manufacturer and get their recommendation.
The peak short-circuit current in bypass path can be calculated based on following equation:
IPEAK_BYPASS is calculated to be 26A based on RBYPASS selected in Equation 25.
The undervoltage lockout (UVLO) can be adjusted using an external voltage divider network of R3 and R4 connected between VS, EN/UVLO and GND pins of the device. The values required for setting the undervoltage and overvoltage are calculated by solving below equation:
For minimizing the input current drawn from the power supply, TI recommends to use higher values of resistance for R3 and R4. However, leakage currents due to external active components connected to the resistor string can add error to these calculations. So, the resistor string current, I(R34) must be chosen to be 20 times greater than the leakage current of UVLO pin.
From the device electrical specifications, V(UVLOR) = 1.24V. From the design requirements, VINUVLO is 24V. To solve the equation, first choose the value of R3 = 470kΩ and use Equation 21 to solve for R4 = 24.5kΩ.
Choose the closest standard 1% resistor values: R3 = 470kΩ, and R4 = 24.9kΩ.