SLUUC56B August 2019 – October 2023 BQ79600-Q1
After configuring all required peripherals on the host microcontroller unit (MCU), begin by pulling nCS low so pings can be sent. Furthermore, MOSI or TX signal from the MCU is used to send wake pings to the MOSI/RX pin of the base BQ79600-Q1. Additionally, send commands that instruct the BQ79600-Q1 to propagate a wake tone to the rest of the stacked BQ79616-Q1 devices.
To calculate the total time to wait, add the WAKE tone duration plus the time to enter ACTIVE mode (total of 11.6 ms) and multiply the result by the number of stacked BQ79616-Q1 devices.
If device is shut down through SHUTDOWN ping, the COMH RX and COML RX are disabled at next wake up. In such case, on step 1, host needs to first send a WAKE ping, wait tSU(WAKE_SHUT) and then send a second WAKE ping. COMH RX and COML RX will be enabled after the second WAKE ping. Then proceed with steps 2 to 4.
Figure 1-2 Wakeup
Flowchart