SLUUCR5A december 2022 – june 2023
Use the following instructions to perform the overcurrent test on the LM74900Q1EVM.
Figure 5-7 and Figure 5-8 show test waveforms for an overcurrent fault.
Figure 5-7 Overcurrent Response of LM74900-Q1 for
a Load Step
From
4 A to 6 A With 5-A Overcurrent Protection Setting
Figure 5-8 Auto-Retry Response of LM74900-Q1 for
an Overcurrent Fault