SLUUCU5 June 2024 TPS544C27
The TPS544C27EVM includes a R7 10Ω series resistor in the feedback loop for VOUT. The resistor is accessible at the test points TP14 (BODE_CHA) and TP8 (VOUT/BODE_CHB) for loop response analysis. These test points must be used during loop response measurements as the perturbation injecting points for the loop . See the description in Table 3-5.
| Test Point | Node Name | Description | Comment |
|---|---|---|---|
| TP14 | BODE_CHA | Input to feedback divider of VOUT | The amplitude of the perturbation at this node must be limited to less than 30mV |
| TP8 | VOUT_BODE_CHB | Resulting output of VOUT | Bode can be measured by a network analyzer with a CHB/CHA configuration |
Measure the loop response with the following procedure: