Use the following instructions to
capture the UVLO behavior of the device.
- Set the input supply voltage VIN
to 25V and current limit of 3A.
- Turn ON the input power
supply.
- Observe the behavior of TG1-IN1
and BG1.
- Turn OFF the power supply and reverse the connection on J1 and J2.
- Observe the behavior of TG2-IN2 and BG2.
Figure 2-2 and Figure 2-3 show examples of the UVLO profile captured on the LM74681EVM evaluation
board.