SLUUDD5 September   2025

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Quick Start Guide
  6. 3Home Screen
  7. 4Starting a New Simulation
  8. 5Running the Simulations and Outputs

Introduction

Ambient light sensors (ALS) and ambient color sensors (ACS) are devices that output a signal proportional to the amount of visible light incident upon the sensing area. When integrating these sensors into product designs, engineers must carefully consider how the entire optical system affects light transmission to ensure accurate measurements across varying conditions. Most product designs require housing the sensor within an enclosure for both protection and aesthetic purposes, as shown in Figure 1-1. However, the physical dimensions and configuration of these enclosures can significantly impact overall optical performance by restricting light paths and altering the sensor's response characteristics.

 Sensor Behind Product
                    Casing Figure 1-1 Sensor Behind Product Casing

In addition to enclosures, designers can choose to include optical materials such as light pipes and cover glass. Many applications use cover glass over sensors for various purposes - for example, dark or tinted cover glass can help conceal the sensor's appearance while still allowing the necessary light transmission for proper operation. This approach maintains the aesthetic design of the product while preserving sensor functionality.

 Dark Cover Glass Figure 1-2 Dark Cover Glass

In instances where the sensor needs to placed deeper within an enclosure, designers can also use light pipes to extend the sensor FOV, as shown in Figure 1-3.

 Light Pipe Figure 1-3 Light Pipe

For complex assemblies, designers might have several layers with window openings, a light pipe, and a diffuser all in the same industrial design to achieve both functional and aesthetic goals. The TI OptiSim tool provides a comprehensive simulation environment that allows designers to evaluate how their complete optical stack-up affects sensor performance. By specifying enclosure dimensions, aperture configurations, and various optical materials, users can accurately model their system's optical characteristics—including angular response and field of view (FOV). This capability enables informed design decisions without requiring physical prototypes or complex simulation software expertise.