A proper layout is critical for the operation of
inverting buck - boost topology. See Figure 4-1 for recommended layout for TPS629210-Q1 inverting buck - boost application.
- The input capacitor C1 should
be placed as close as possible between the VIN pin and GND.
- The output capacitors C2, C4,
C5 should be placed as close as possible between -VOUT pin and
GND.
- VOS trace should be
routed/Kelvined to the positive terminal (GND) of output capacitors, not
simply tied to the system GND plane.
- Sensitive nodes like FB/VSET
and VOS need to be connected with short wires and not nearby high dv/dt
signals( like SW). As they carry information about output voltage, they
should be connected as close as possible to actual output voltage (at the
pad of output capacitor). For this design, there is no feedback resistors
required (float the FB/VSET pin) resulting in a -3.3V output voltage using
the internal VSET.
- MODE/S-CONF pin resistor R3
should be kept close to IC and connect directly to its pin.