SLVAG32 June   2026 TPS7B7702-Q1

 

  1.   1
  2.   Abstract
  3. 1Profile of TPS7B7702
  4. 2Vsense Waveform
  5. 3Reverse Overcurrent Protection
  6. 4Conclusion
  7. 5References

Profile of TPS7B7702

The TPS7B7702-Q1 is an antenna LDO that supports a wide input voltage range (4.5-40V). It can be connected directly to a 12V battery input (to adapt to voltage fluctuations caused by conditions such as cold boot or load dump). It commonly supplies a stable voltage output via coaxial cables to loads such as low-noise amplifiers in active antennas. It offers excellent diagnostic and protection features, using the sense and Error pins to characterize failures such as output short-circuit, output short-to-battery, overtemperature, and reverse current. Its sense pin can also characterize the current actually flowing by mirroring the current source, which helps customers save on external shunt resistors without affecting the LDO's dropout voltage. The following figure shows a typical application circuit.

 TPS7B7702-Q1 Typical Application Block DiagramFigure 1-1 TPS7B7702-Q1 Typical Application Block Diagram

There are a few points to note when designing the actual circuit, which are introduced in the corresponding sections of the reference datasheet:

  1. For the input capacitor, the datasheet recommends a nominal value of 10uF and does not specify a minimum effective capacitance. The input capacitor is intended to prevent the triggering of undervoltage protection due to output voltage dropping during load transients. In general, when the input supply impedance is greater than 0.5 ohms, an input capacitor is required. For a dual-channel LDO like the 7702, when one channel's output is shorted to ground, the energy stored in the input capacitor is momentarily drawn, causing a transient drop. This may trigger reverse overcurrent protection on the other channel, thereby affecting its normal operation. Considering this condition, a larger input capacitor would be better.
  2. The dual-channel LDO can also be connected in parallel to increase current capability. TI offers a reference design, TIDA050096, for reference. This device can also be used in single-channel mode; the corresponding EN pin can be left floating, as there is an internal pull-down on the pin. Unused pins can be left floating or connected to ground. Grounding is recommended to improve the thermal dissipation of the chip.
  3. In the EVM for this device, a ferrite bead is placed at the output, similar to the figure above. This bead is not required and is originally intended to simulate an inductive clamping feature. Placing a bead is also fine, which essentially adds an extra stage of LC filtering.