SLVK230 November 2025 TPS7H4102-SEP
The TPS7H4102-SEP is packaged in a 64-pin plastic package as shown in Figure 3-1. The TPS7H4102EVM was used to evaluate the performance and characteristics of the TPS7H4102-SEP under heavy ion radiation. The TPS7H4102EVM is shown in Figure 3-2. The schematic is shown in Figure 3-3. For further detail please reference the TPS7H4102EVM User's Guide.
Note for the VOUT=1.2V case both outputs were configured similar to VOUT1 and for the VOUT=1.8V case both outputs were configured similar to VOUT4. Please refer to Table 6-2 for a breakdown of component values.